mpxy8300 interrupt illegal_bp problem

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

mpxy8300 interrupt illegal_bp problem

940 Views
nemanjasavic
Contributor I

Hi all guys,

 

I am currently working on a project using MPXY8300 TPMS chip, which is driven by HSC08 core. However I have encountered problem when using interrupts, and I always get ILLEGAL_BP while debugging. I have read several posts but nothing actually helped me. Here is what I have:

 

void main(void) {   /* This code continously transmit TPMS packets of type BERU RDE012 */      UINT8 i;   volatile UINT8 tmp;   volatile UINT8 RFRD_data[11];   UINT16 delay=0;      /* Set up MCU and set STOP mode. */   __RESET_WATCHDOG();      vfnSetupMCU();   vfnSetSTOPMode(4);    vfnSetupRFX();      EnableInterrupts;        PTADD |= BIT3;  // set pin A3 output    LED_OFF;   LED_ON;   LED_OFF;   while(1); } 

 

COP is disabled by writing 0x33 in SOPT1 reg.

Interrupt is defined in another file in the following way:

#pragma CODE_SEG NON_BANKED void interrupt VectorNumber_Vwuktmr wup_isr(void) {   PWUCS0_WUFACK = SET;  PWUCS1_PRFACK = SET;   LED_ON;  LED_OFF; } #pragma CODE_SEG DEFAULT

 

I don't use any interrupt table (If I understood correctly,that was an old way, but I also tried with linking error that desired segment is already in use ...).

 

Many thanks in advance for your suggestions,

Nemanja Savic

Labels (1)
Tags (2)
0 Kudos
Reply
0 Replies