microcontroller does not allow new programming

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

microcontroller does not allow new programming

1,732 次查看
oscarm
Contributor I

hi, i'm using a mc9s08gt60a microcontroller and it was working without problems, leting making new programming several times, but in a moment it doesn't allow a new programming, and i didn´t use the security bit, but when codewarrior try to program, it shows an advice that says that the microncontroller may be secured.



Message Edited by oscarm on 2008-05-25 10:07 PM
标签 (1)
0 项奖励
回复
1 回复

997 次查看
Witztronics
Contributor IV
Did you try to use the unsecure command in the debugger menu?

It depends which debugger you are using, but there should be a menu named after the debugger, like "Open Source BDM" or something like that.  In that menu should be an unsecure command.
0 项奖励
回复