microcontroller does not allow new programming

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

microcontroller does not allow new programming

1,789件の閲覧回数
oscarm
Contributor I

hi, i'm using a mc9s08gt60a microcontroller and it was working without problems, leting making new programming several times, but in a moment it doesn't allow a new programming, and i didn´t use the security bit, but when codewarrior try to program, it shows an advice that says that the microncontroller may be secured.



Message Edited by oscarm on 2008-05-25 10:07 PM
ラベル(1)
0 件の賞賛
返信
1 返信

1,054件の閲覧回数
Witztronics
Contributor IV
Did you try to use the unsecure command in the debugger menu?

It depends which debugger you are using, but there should be a menu named after the debugger, like "Open Source BDM" or something like that.  In that menu should be an unsecure command.
0 件の賞賛
返信