mc9s08qg8 compiler

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

mc9s08qg8 compiler

245 Views
joepuhich
Contributor I

proto type: i have a product using this chip. it is not obsolete. i have the code to compile, from 1980. what i want to do, is update the cs v6.3 code on windows 11. i want to update the product from and evaluation unit to a working unit, to be released to manufacturers of sewing equipment. I have three lines of c code to update the product for production.  HISTORY: BOBBIN SHOW < 1980. displayed prototype of unit at the show and sold 15 copies for $150 each. I developed specialized gate array chips at International Microciruits INC(IMI) to implement functions. WELL, the unit was a single use. I got a patent and I put the  BOBBIN CONTROLLER "BC" away until 1983.  Used the mc9s08qg8 chip to up grade the BC to many more functions. living on welfare, i did not have money to further my business. NOW i took the developed unit out of storage, and being 72 i am trying to finish off the last coding to get the latest functions. i am going to try to sell it big before i die. my last move before i die, i can not loose. If u can not help me further, i am going to TI and use their chips. U have me locked out of your devlopment software. So i got maybe 12 years left, and ur chip is the core of the product. If U R not intersested in this product, i will go to TI. I do not have time to play with you business cycles. I figure if the unit takes off, i can sell 20,000 units. It works better than i tought 43 years ago, So am I in or out. I need the BDM drive for my wiztronics. com board interface and cw 11.1 to finish the final unit off. ALSO, i am still on SS. NO money, only a dream. i can not afford $500 fora P&E USB multilink Universal prgrammer. Maybe u would like to "venture capital" the device. u got the whole c code, which i downloaded to u!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!! the ball is in ur court.

 

0 Kudos
Reply
1 Reply

198 Views
luis_maravilla
NXP Employee
NXP Employee

Hello

I give you a suggestion on your other post if it could help you in repairing the BDM driver to use the device in CodeWarrior

mc9s08qg8 drivers

Could you confirm if you have consulted with Wiztronics about the driver's usage in their boards, do you have any feedback?

Best Regards

0 Kudos
Reply