mc9s08qg8 drivers

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

mc9s08qg8 drivers

372 Views
joepuhich
Contributor I

device manager:

Jungo connectivity

WinDriver:      Windows cannot verify the digital signature for the drivers required for this device. A recent hardware or software change might have installed a file that is signed incorrectly or damaged, or that might be malicious software from an unknown source. (Code 52)

 
pemicrowindvr:    This device is working properly.
 
These r the drivers i have in jungo!!!
 
ur input:
 
In USB Multilink Universal and USB Multilink Universal FX Technical Summary [USBMLUNIVERSALFX] documentation Chapter 6 Driver Installation mention that a copy of the driver installation program may be downloaded from P&E page "Support Center">Downloads. if you need an updated driver.   Best Regards,
 
What do u mean by this. Is this where i can get my BDM driver for my Wiztronics.com P&E interface board?
0 Kudos
Reply
1 Reply

334 Views
luis_maravilla
NXP Employee
NXP Employee

Hello,

From the other post, I was referring that, as you are using P&E USB multilink Universal, the support page could redirect you to download a patch or an upgrade to your driver, I found these resources that could maybe help you if you have an incorrectly driver.

In these page, its mentioned some patches for CodeWarrior v10.2 or higher and v6.3, to add support for PE hardware if is not detected by the operating system. PEmicro FAQ ID 211

Another option USB Multilink Resources Install Is a resource package for USB Multilink Universal, for when running older software.

Also could you help us share which exact version of USB multilink Universal are you using?

I could not guarantee this will work, since it’s a partner page, but it could redirect you in how to look for a driver correction for your issue, hope this information was helpful and let me know if that work for you

Best Regards.

0 Kudos
Reply