mc68hc908gp32 init error

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

mc68hc908gp32 init error

1,605 次查看
olivier_quebec
Contributor I
Hi, it is not the first time i am burning a gp32 but it is the first time with this new pcb and the first time on the computer i am using for the task. I do it with ide codewarrior. At the moment, there is nothing in the program, i am just trying to enter monitor mode. After  codewarrior ask me if i want to erase the flash memory and i answer yes, the following error happens: --initializing  unable to access processor
                                                                                            error 35 during script
 
Thank you for reading this.
 
Olivier Allaire
 
 
 
 
标签 (1)
0 项奖励
回复
1 回复

969 次查看
peg
Senior Contributor IV
Hello Olivier and welcome to the fora.

So you get past the initial connection dialogue but then get stuck when it tries to erase. Is this correct?
What MON08 adapter are you using? What class is it?
Are you using a "real" serial port on your computer or a USB adapter or someting?
Perhaps try going into "Expert mode" where you can try a few other things to see what happens.

0 项奖励
回复