mc68hc908gp32 init error

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

mc68hc908gp32 init error

1,574 Views
olivier_quebec
Contributor I
Hi, it is not the first time i am burning a gp32 but it is the first time with this new pcb and the first time on the computer i am using for the task. I do it with ide codewarrior. At the moment, there is nothing in the program, i am just trying to enter monitor mode. After  codewarrior ask me if i want to erase the flash memory and i answer yes, the following error happens: --initializing  unable to access processor
                                                                                            error 35 during script
 
Thank you for reading this.
 
Olivier Allaire
 
 
 
 
Labels (1)
0 Kudos
Reply
1 Reply

938 Views
peg
Senior Contributor IV
Hello Olivier and welcome to the fora.

So you get past the initial connection dialogue but then get stuck when it tries to erase. Is this correct?
What MON08 adapter are you using? What class is it?
Are you using a "real" serial port on your computer or a USB adapter or someting?
Perhaps try going into "Expert mode" where you can try a few other things to see what happens.

0 Kudos
Reply