mc68hc908az60

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

mc68hc908az60

1,708 Views
fabricepeden
Contributor I

Hi everybody,

I got a problem with microcontrollers MC68HC908AZ60.

I got a binary that works well on a MC68HC908AZ60. I bought some "new" microcontrollers MC68HC908AZ60A, I red the differences between both µc (cf. AN2215), and try to modify some registers in my binary file but it doesn't work.

Is there a document or a method to migrate a software from MC68HC908AZ60 to MC68HC908AZ60A ?

Thank you in advance,

Fabrice

Tags (1)
0 Kudos
Reply
2 Replies

1,556 Views
miduo
NXP Employee
NXP Employee

Hi, Fabrice

I saw you had put another case to our support system and it had been assigned already. I am pretty sure you will receive the response soon.

PS: please put any 8 bit MCU issue within the according community, here is just for ColdFire. Thanks.

0 Kudos
Reply

1,556 Views
TomE
Specialist II

The "MC68HC908AZ60" is not a ColdFire processor.

Please move your question to the following Forum, and also search that Forum for any relevant answers.

As well as that App Note, the differences are also listed in Appendix A in the MC68HC908AZ60A Data Sheet.

The Flash and EEPROM have changed a lot. Control Registers have moved and the clock setup (for the EEPROM) is different.

You really need to recompile the original source code with appropriate changes. If you don't have the source (and the compiler and development system, computer old enough to run it, operating system old enough to run it, working licenses) then the only option to make reliable products is to use the Non-A parts.

Tom

0 Kudos
Reply