mc68hc908ap32 Monitor Mode Debugging

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

mc68hc908ap32 Monitor Mode Debugging

1,160件の閲覧回数
kuraga200
Contributor II

Hello, how i can exit monitor MODE and run code IN user MODE without POR (eq. power-of-reset)?

I trying save stack&RAM variables which wrote while MCU in monitor mode, and start user code in user mode.

I try to create little subroutine for debugging MCU in Monitor mode. I read an2295 but i don't want to use this way because need to re-burn MCU with bootloader.

(sorry for my English)

I not fully understand what is exactly Monitor mode - this is some special kind of interrupt or subroutine and i can return to user mode with my variables etc. or this is some hardware module, and i can't do any actions (beside hardware) to back in user mode.

ラベル(1)
タグ(3)
0 件の賞賛
返信
0 返答(返信)