long multiplication issues

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

long multiplication issues

跳至解决方案
1,652 次查看
thomasj
Contributor I

Hello

 

I am currently working on a MC9S08SH8 with CodeWarrior IDE 5.9.0( build 5292 ) to design an interface between 2 sub-systems. One collects data, and the other sends them. My program is to read the data received, convert them into SI units (meters, Pascals ... ) and store them in a 32 bytes vector in order to send data through RS-232 serial port.

Problem is, during the conversion phase, some multiplications are done wrong :

 

This one works perfectly :

     unsigned short valor = 30000;

   

     unsigned short resultado;

     unsigned long temp;

 

     temp = (valor*33782);

     auxiliar_1 = temp;     // = 1.013.460.000

 

     resultado = temp;

 

 

But this one does not :


     unsigned short valor = 300;   


     unsigned short resultado;

     unsigned long temp;

  

     temp = (valor*254);

     auxiliar_2 = temp;     // = 10.664 instead of 76.200 !

 

     resultado = temp;



I have noticed that 76.200d is 1 00101001 10101000b in binary,

                     and 10.664d is 0 00101001 10101000b.


So it seems that even though temp is a long type(4 bytes), in the second example, it is truncated to short type(2bytes), but not in the first ...

Any idea why this happens ? Syntaxis and call situation are identical. I tried replacing the "254" in the second example by "33782" and it worked. How could it be related to the number ?


Thanks in advance,

Thomas

 

 


标签 (1)
0 项奖励
回复
1 解答
1,500 次查看
bigmac
Specialist III

Hello Thomas,

Try the following -

temp = (valor * 254UL);

This should cause the result of the multiplication to be 32-bit, rather than 16-bit.

Regards,

Mac

在原帖中查看解决方案

0 项奖励
回复
2 回复数
1,501 次查看
bigmac
Specialist III

Hello Thomas,

Try the following -

temp = (valor * 254UL);

This should cause the result of the multiplication to be 32-bit, rather than 16-bit.

Regards,

Mac

0 项奖励
回复
1,500 次查看
thomasj
Contributor I

Thank you very much !

I had tried with a cast on my own shortly after posting that(ocurred like this :smileysilly:) and it worked as well.

Your way is "cleaner" than a cast on "valor", that's probably what I'll use.

Again, thanks, problem solved

Thomas

0 项奖励
回复