load the program into a HCS08 without CodeWarrior

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

load the program into a HCS08 without CodeWarrior

跳至解决方案
3,553 次查看
hasaur
Contributor II

Hello,

 

I would like to know if it is possible the load the program into a HCS08 (I have a MC9S08DZ128, with CAN) without CodeWarrior. I would like to use a Java app to load it. Is there a solution ??

 

Thank you in advance.

标签 (1)
0 项奖励
回复
1 解答
2,612 次查看
J2MEJediMaster
Specialist I

I am not sure if you are trying to debug the program or just simply load it onto the processor for testing. PE Microsystems has some devices that can be used to download programs onto the part without the use of CodeWarrior. I do not think they use Java, however.

 

---Tom

在原帖中查看解决方案

0 项奖励
回复
3 回复数
2,612 次查看
Witztronics
Contributor IV

I'm not sure if this will work for your project, but you can use Hiwave to program a part without launching Codewarrior.

 

1)      Create a new shortcut by right clicking on the windows desktop.

2)      Browse to Hiwave.exe as the target application (normally in the

         C:\Program Files\Freescale\CodeWarrior for Microcontrollers V6.2\prog directory)

3)      After the shortcut has been added, right click on the new shortcut to edit it’s properties.

4)      Under the “shortcut” tab, modify the target settings to include the program file and target debugger.

 

Example: "C:\Program Files\Freescale\CodeWarrior for Microcontrollers V6.2\prog\hiwave.exe" C:\ myfile.s19 -Target=HCS08OpenSourceBDM

 

5)      Select “OK” to close the shortcut properties box.

 

Double clicking on the Hiwave shortcut you created will now launch the Hiwave debugger and program "myfile.s19" into the device attached to the “HCS08OpenSourceBDM” (WTBDMS08).

 

The other option is to use the S08 programmer written by PGO and the USBDM.. 

https://community.freescale.com/thread/60277

 

0 项奖励
回复
2,613 次查看
J2MEJediMaster
Specialist I

I am not sure if you are trying to debug the program or just simply load it onto the processor for testing. PE Microsystems has some devices that can be used to download programs onto the part without the use of CodeWarrior. I do not think they use Java, however.

 

---Tom

0 项奖励
回复
2,612 次查看
hasaur
Contributor II

thanks you a lot.

I think it could work with Java because there are DLL.

I thought that another product wasn't necessary.

Thank you.

0 项奖励
回复