is therr a bootloader in qg8?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

is therr a bootloader in qg8?

3,065件の閲覧回数
HarrySun
Contributor I
Hello,
 
I could not program/debug a blank QG8 bought from freescale on my own board,via a P&E USB mulitlink, while I could do this on qg8 demo board,DEMO9S08QG8.
so when I need to program/ debug a blank qg8, I first put it on the demo board and program it with any code such as demo code ,put it back on my own board,then  I can debug/program it.
can anybody tell me why?is there a bootloader being downloaded to a blank qg8 on a demo board while it doesn't do the same thing on my own board??
 
thanks very much
Harry
ラベル(1)
0 件の賞賛
返信
3 返答(返信)

1,753件の閲覧回数
peg
Senior Contributor IV
Hi HarrySun,
 
There is nothing progammed into a fresh from the factory QG.
The QG has to be handled differently when blank which I believe the demo board assists with.
See this thread about this problem:
 
 
0 件の賞賛
返信

1,753件の閲覧回数
HarrySun
Contributor I
Peg,
 
well said,I appreciate it very much.
on the other hand , I am not convinced that this is  a fully debugged design,for example, why should 0XFF be used as an instruction,STX,X??which makes things worse...
Have a nice day
 
 
0 件の賞賛
返信

1,753件の閲覧回数
peg
Senior Contributor IV


HarrySun wrote:
Peg,
 
well said,I appreciate it very much.
on the other hand , I am not convinced that this is  a fully debugged design,for example, why should 0XFF be used as an instruction,STX,X??which makes things worse...
Have a nice day
 
 


Hi HarrySun,
 
The use of this value for this opcode has a heritage stretching back for over 20 years. I doubt they are going to change it now.

 
0 件の賞賛
返信