interfacing spi

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

interfacing spi

Jump to solution
8,346 Views
roberto_m
Contributor III

Hi to all, do you think it is possible link 4-wires SPI on my qe64 to 3-wires spi of "si4432" (silicon labs)?

Labels (1)
0 Kudos
Reply
1 Solution
6,304 Views
peg
Senior Contributor IV

Hello Roberto,

 

As this interface is synchronous the master can stop/start/change speed whenever it feels like it and the slave end will just follow the clock and read the input/set the output at the appropriate time. So the pause is not an issue.

However by properly utilising the buffered nature of the SCID you can join the data stream together.

 

Example:

 

  PTBD_PTBD5 = 0;// enable ss  while (!SPI1S_SPTEF); // wait transmit buffer empty flag    SPI1D = address;  // send address  while (!SPI1S_SPTEF); // wait transmit buffer empty flag    SPI1D = data;    // new data  while (!SPI1S_SPRF);  // wait      SPI1D;       // clear flag  while (!SPI1S_SPRF);  // wait      SPI1D;       // clear flag  PTBD_PTBD5 = 1;    // disable ss

 

 

By always waiting until the SCID is truly MT in the routine, the SCID transmit side will always be truly MT (both shift register and buffer) when you enter the routine. This allows you to stuff two bytes before you start reading. This scheme can be extended to produce a longer continuous stream.

 

Happy SPIing

 

View solution in original post

0 Kudos
Reply
14 Replies
6,304 Views
bigmac
Specialist III

Hello Roberto,

 

In fact the SI4432 device does require four connections for the SPI interface.

SDI <-> MOSI

SDO <-> MISO

SCLK <-> SPCLK

nSEL <-> (SS)

 

nSEL may connect to any GP output pin, and must be controlled by your code.  If you choose to use the SS pin, this will also need to be configured as GP output.  Automatic operation of the SS output is not appropriate because of the multiple byte commands required by the transceiver device.

 

Regards,

Mac

 

0 Kudos
Reply
6,304 Views
roberto_m
Contributor III

Thank you, I have read the data sheet, and I come to the same end. The only «doubt» is on the behaviour of SDO, but in short I think i could try it...

 

Regards,

roberto

0 Kudos
Reply
6,304 Views
roberto_m
Contributor III

Hi, now I'm trying to connect it... using SPI on my qe64.
I need to realize a timing like in figure.
I'm using these settings:

  SPI1C1 = 0x50; // master mode CPOL = CPHA = 0, ssoe = 0
  SPI1C2 = 0x00; // modfen = 0 => ss = gpio

and this routine:

void spi_write_register (unsigned char address, unsigned char data)
 {
  __asm SEI;
  PTBD_PTBD5 = 0;// enable ss
  while (!SPI1S_SPTEF); // wait transmit buffer empty flag 
   SPI1D = address;  // send address
  while (!SPI1S_SPRF);  // wait
      SPI1D;       // clear flag
   SPI1D = data;    // new data
  while (!SPI1S_SPRF); // wait
  PTBD_PTBD5 = 1;    // disable ss

  __asm CLI;
 }

I'm getting something similar at the figure attached. But, between bit a0 and bit d7,
i have an extra-pause. How can I kill it?

If someone could help me, thanks a lot,
Best regards
Roberto

0 Kudos
Reply
6,305 Views
peg
Senior Contributor IV

Hello Roberto,

 

As this interface is synchronous the master can stop/start/change speed whenever it feels like it and the slave end will just follow the clock and read the input/set the output at the appropriate time. So the pause is not an issue.

However by properly utilising the buffered nature of the SCID you can join the data stream together.

 

Example:

 

  PTBD_PTBD5 = 0;// enable ss  while (!SPI1S_SPTEF); // wait transmit buffer empty flag    SPI1D = address;  // send address  while (!SPI1S_SPTEF); // wait transmit buffer empty flag    SPI1D = data;    // new data  while (!SPI1S_SPRF);  // wait      SPI1D;       // clear flag  while (!SPI1S_SPRF);  // wait      SPI1D;       // clear flag  PTBD_PTBD5 = 1;    // disable ss

 

 

By always waiting until the SCID is truly MT in the routine, the SCID transmit side will always be truly MT (both shift register and buffer) when you enter the routine. This allows you to stuff two bytes before you start reading. This scheme can be extended to produce a longer continuous stream.

 

Happy SPIing

 

0 Kudos
Reply
6,304 Views
roberto_m
Contributor III

it works! thank you Peg, thank you Big Mac.

 

Regards,

Roberto

0 Kudos
Reply
6,304 Views
roberto_m
Contributor III

Hi,

again on this.

If I use SPI communication between mcu and transceiver with Prescaler 8 (1:1:1) and Rate Divisor 4 (0:0:1) (f_bus = 20 Mhz => sclk = 625 khz) it works everything. But I  have a lot of data so I think to speed up communication with Prescaler 8 and Rate divisor 2 (0:0:0) (sclk = 1,25 Mhz ). With this baud rate the transceiver doesn't trasmit. With an oscilloscope I see a normal SPI communication between devices but there is transmission.

Any suggestion?

0 Kudos
Reply
6,304 Views
bigmac
Specialist III

Hello Roberto,

 

As Peg has already suggested, if you are using the code that utilizes the double buffering capability of the SCI module, it is possible for an overrun condition to occur, where the transmission of the second byte is completed before the first byte can be read.  Data will be lost.  For the original SPI clock rate, the value of the first received byte must be read within less than 256 bus cycles from the completion of the transfer.  By doubling the SPI clock rate, the critical read period would be halved to 128 bus cycles.

 

It is therefore possible that a timer, or other interrupt may occur at the critical point, and may take more than 128 cycles to complete execution.

 

Solution 1:  Globally disable interrupts just prior to sending the second byte, and re-enable interrupts after the first byte has been read, and the flag cleared.

 

Solution 2:  Do not send the second byte until after the first byte has been read.  This will eliminate any critical timing.

 

Regards,

Mac

 

0 Kudos
Reply
6,304 Views
peg
Senior Contributor IV

Hello Roberto,

 

I'm not sure I am understanding you.

Are you saying you have a working setup and then when you speed up the SPI clock it stops working?

You are seeing the data on the SPI lines but it is not working?

 

A not on the code presented previously:

This style of SPI code is generally not used as it is not interrupt proof.

It relies on being able to load both bytes before the first one has completely shifted out.

Indeed single stepping the routine will cause it to hang.

You could disable interrupts during the critical stage but you have to ask yourself whether you really need those back to back transmissions. With enough differential between buss clock and SPI clock speeds you get it anyway.

 

0 Kudos
Reply
6,304 Views
roberto_m
Contributor III

@PEG  Yes I had a working setup and speed up action stopped all.

 

I disable interrupts and it works.

 

I use this new routine:

 

  SS = 0;        // enable SS
   while (!SPI1S_SPTEF); // wait: "transmit buffer empty flag"
     SPI1S;
     SPI1D = address;
  while (!SPI1S_SPRF);  // wait: "reader buffer full flag"
     SPI1S;      // clear flag
     SPI1D;
     SPI1D = data;                               
   while (!SPI1S_SPRF); // wait: "reader buffer full flag"
      SPI1S;
      SPI1D;           // clear flag
   SS = 1;          // disable SS

It works with or without interrupts.

Thank you for all Peg and Bigmac,

 

Regards.

 

Roberto 

0 Kudos
Reply
6,304 Views
peg
Senior Contributor IV

Hello Roberto,

 

Glad you got it sorted out.

The additinal SPI1S reads (SPI1S:smileywink: should not be required.

You are doing a read in the flag test line above it.

 

0 Kudos
Reply
6,304 Views
roberto_m
Contributor III

If i remove additional reads to SPIS it doesn't work...:smiley sad:

0 Kudos
Reply
6,304 Views
peg
Senior Contributor IV

Hi,

Must be due to a timing issue at the other end then.

 

0 Kudos
Reply
6,304 Views
bigmac
Specialist III

Hello Roberto,

 

The slight delay is due to the fetching of the data byte following the transmission of the address byte.  This is of no consequence since the next clock pulses generated by the master is also delayed.  On the same basis, it is usually unnecessary that interrupts need to be disabled and re-enabled.

 

Are you able to operate the SPI device as intended?

 

Regards,

Mac

 

0 Kudos
Reply
6,304 Views
peg
Senior Contributor IV

Hello,

 

Yes this is possible. The SS signal is very much optional.

Connect the clocks MOSI MISO together ans set one as master the other as slave and off you go!

 

0 Kudos
Reply