hello, I am using cpu MC9S08SE8VWLE, please which kind of programmer I will use? I used PE MIcro, but I do not like it, is there a cheaper NXP device to use? thanks

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

hello, I am using cpu MC9S08SE8VWLE, please which kind of programmer I will use? I used PE MIcro, but I do not like it, is there a cheaper NXP device to use? thanks

2,652 次查看
henryscott
Contributor I

hello, I am using cpu MC9S08SE8VWLE, please which kind of programmer I will use? I used PE MIcro, but I do not like it, is there a cheaper NXP device to use? thanks

标签 (1)
0 项奖励
回复
4 回复数

2,498 次查看
tonyp
Senior Contributor II

You can use the very low cost open source USBDM programmer.  Google it and also on eBay.

0 项奖励
回复

2,498 次查看
henryscott
Contributor I

hello,

I have ordered on Amazon, by OVJ a USBDM programmer, ASIN B07KSD2SFF.

I can't find many informations about it, do you think I can use hiwave

software to program the MC9S08SE8VWLE?

thanks

Henry

Il 06/02/2019 22:25, tonyp ha scritto:

USBDM programmer.

0 项奖励
回复

2,498 次查看
henryscott
Contributor I

so many thanks, when I will receive programmer fron Amazon, I check it.

HEnry

Il 07/02/2019 22:25, tonyp ha scritto:

>

NXP Community

<https://community.freescale.com/resources/statics/1000/35400-NXP-Community-Email-banner-600x75.jpg>

>

Re: hello, I am using cpu MC9S08SE8VWLE, please which kind of

programmer I will use? I used PE MIcro, but I do not like it, is

there a cheaper NXP device to use? thanks

reply from Tony Papadimitriou

<https://community.nxp.com/people/tonyp?et=watches.email.thread> in

/8-bit Microcontrollers/ - View the full discussion

<https://community.nxp.com/message/1110451?commentID=1110451&et=watches.email.thread#comment-1110451>

>

0 项奖励
回复