flash programming of the DEMO908GZ60

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

flash programming of the DEMO908GZ60

2,258件の閲覧回数
johndoe64
Contributor I
Hello,
i am fighting with the flash programming of the DEMO908GZ60.
I am using CW3.1 with the HC908GZ60 Patch.
I carefully read all the messages concerning DEMO908GZ60 Flash programming in the 8 Bit Processors forum.
I followed the instructions of the DEMO908GZ60 Quick start Guide, double-cross checking the settings for serial connection, making sure the COM Port matches the setting and connected. My Volt Meter shows a perfect 9V Level on the terminal power block.
I checked the IGNORE box.
I followed the instructions on the screen and i clicked the YES button.
I cycled the power as requested, shorting the terminal power block to ensure less than 0.1Volts, but then instead of programming the flash, the program tells me: "Device responds properly, but ROM is secured: error 35"
I understand very well that with a secured ROM it is not possible to flash the device but how can i unsecure it?

Please help
ラベル(1)
0 件の賞賛
返信
2 返答(返信)

1,192件の閲覧回数
Ake
Contributor III
By the way, did you set the baud rate to 7200 baud?
 
Regards,
Ake
0 件の賞賛
返信

1,192件の閲覧回数
Ake
Contributor III
Hi,
Here is a HC908GZ60 Flash programming program that I wrote some time ago.
I ran it on a DEMO908GZ60 board and it seems to be OK.
 
I cannot guarantee that it is free from errors, at least I did not see any.
 
Regards,
Ake
 
Message Edited by t.dowe on 2009-10-27 01:58 PM
0 件の賞賛
返信