exp,log and other math functions using CW for MCU Development Studio v10.6 and an MC9S08PA8

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

exp,log and other math functions using CW for MCU Development Studio v10.6 and an MC9S08PA8

3,481件の閲覧回数
efthymioskondos
Contributor II

Dear community,

I am transfering a part of code from one MCU vendor (Atmel xmega32E5) to Freescale/NXP MC9S08PA8 MCU ,

and when I use the log function from math.h (i hope like other IDEs does)  the MCU "hits" endless restarts.

If i comment this line, MCU does its supposed job without any issue and i can see an ADC result on debugger crystal clear.

 

unsigned int temp;

double ftemp;

 

void main(void)

{

  System_Init();                                            //Initialise system hardware/software modules

 

  for(;;)

  {

  temp=ADC_Get_Sample(CH11);              //Read current channel ADC value (54us@8MHz)

  ftemp=log(((10240000/temp) - 10000));   //Endless restart occurs - CRITICAL point

  }

}

 

1) How /When do i  update/include the "math.h" or similar (?) library header ?

2) Does this IDE support floats and doubles for "small ones" like the PA16 MCU?

(I have chosen at the beggining bareboard project with IIEE 64bit float support)

 

Best Regards,

Tim

ラベル(1)
4 返答(返信)

3,198件の閲覧回数
efthymioskondos
Contributor II

FIY ,

SOLVED according to Edward Karpicz and Stanislav suggestion.

So to use logx,log , exp functions , include your <math.h> on your project and also go to

Project Settings->Linker_Files->Project.prm , open file with double click

and edit  STACKSIZE from 0x80 (128bytes default size), to a bigger numer.
But beware, not to kill the entire RAM area by entering exotic hex number (For me it worked for 256bytes (0x100).

Cheers,

Ef

0 件の賞賛
返信

3,198件の閲覧回数
efthymioskondos
Contributor II

Thank you Edward & Stanislav for your fast response ,

I will look into it as for math.h and modify(increase) the stack size of S08.

See how it goes, and get you feedback as soon as possible.

Cheers,

Tim

0 件の賞賛
返信

3,198件の閲覧回数
kef2
Senior Contributor V

Default stack size set in PRM file is too short for S08 math functions.

3,198件の閲覧回数
Stano
NXP Employee
NXP Employee

Hello Efthymios,

it is possible to use the math functions in CW10.6. You need just include it:

#include <math.h>

It adds the math.h file from the installed CW package.

I hope this helps you.

Best Regards,

Stano.