example code for 9s08mm128 CMT module

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

example code for 9s08mm128 CMT module

1,832 Views
farnellzhang
Contributor I

Dears,

is there any example code for 9s08mm128 CMT module? i am working FSK modulation on MM128 device, and i can not find any demo code of CMT module.

can anybody help me, please?

i am appropriated for your support!

 

best regards,

 

oliver zhang

Dec 26,2014

Labels (1)
0 Kudos
Reply
2 Replies

1,648 Views
vicentegomez
NXP TechSupport
NXP TechSupport

Hi Oliver

Please check the application note AN3053 " Infrared Remote Control Techniques on MC9S08RC/RD/RE/RG Family" on it you can find a description of how to use the CMT module (also a sample code), the module on the MC9S08RC and the MC9S08MM are the same.

I hope this will help you.

Have a great day,
Vicente

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

1,648 Views
Luis_Garabo
NXP TechSupport
NXP TechSupport

Hi,

I have moved your question to the community where you will get support on your issue.

If you have more questions related to this Freescale Product part then please post them in this community where This thread was moved.

Have a nice day.

Best Regards,

Garabo

0 Kudos
Reply