debug break on ADC S08PT60

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

debug break on ADC S08PT60

1,277件の閲覧回数
IlConte
Contributor IV

I use a S08PT60 with code warrior 10.6 and multilink pemicro debug

I use the ADC converter configured without interrupt (ADC_SC1 = 0b00000000;)

 

When the coco bit is set, i restart the conversion eith other channel :

  if (ADC_SC1_COCO)

    {

    switch (ADC_SC1 & 0x1F)

      {

      case 0:

        First = ADC_RL;

        ADC_SC1 = 1;

        break;

 

      case 1:

        Second = ADC_RL;

        ADC_SC1 = 0;            

        break;

   }

 

When with cw, I suspend the excexution, the ADC crashes and the coco bit remain low.

When crash the ADC register value is the follow

 

ADC_SC1    0x01    0x0010   

ADC_SC2    0x08    0x0011   

ADC_SC3    0x00    0x0012   

ADC_SC4    0x00    0x0013   

ADC_RH    0x00    0x0014   

ADC_RL    0x39    0x0015   

ADC_CVH    0x00    0x0016   

ADC_CVL    0x00    0x0017   

ADC_APCTL1    0x03    0x30ac   

ADC_APCTL2    0xf0    0x30ad   

 

 

I have this problem only if break, without break all goes !

 

I would like to understand why, and fix this annoying problem


Thanks


Stefano

ラベル(1)
0 件の賞賛
返信
2 返答(返信)

1,130件の閲覧回数
vicentegomez
NXP TechSupport
NXP TechSupport

Hi Stefano

Would be possible that you send me a project to reproduce the problem?

Thanks in advance


Have a great day,
Vicente

0 件の賞賛
返信

1,130件の閲覧回数
IlConte
Contributor IV

Solved with new project, thanks

0 件の賞賛
返信