clean  transmit buffers - MC9S08QE128

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

clean  transmit buffers - MC9S08QE128

1,499 Views
shumpi55
Contributor I
I am using MC9S08QE128 microcontroller(HCS08)
how can i clean the transmit buffer so that I can transmit data using SCi at regular intervals?
 
 
 
 
 
 
 
 
 
Added p/n to subject.


Message Edited by NLFSJ on 2008-07-30 02:16 PM
Labels (1)
0 Kudos
Reply
1 Reply

779 Views
peg
Senior Contributor IV
Hi shumpi,

There is no need to clear the transmit buffer.
just write something in there and it will be transmitted.
Why do you feel you need to clean it?
The initial enable is covered by it using a pre-amble byte, which should be undetectable in operation.

0 Kudos
Reply