binding process  - MC13224V rev 2.1

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

binding process  - MC13224V rev 2.1

ソリューションへジャンプ
2,383件の閲覧回数
tpicon
Contributor II

Hi 

 

I have a coordinator node (MC1322x Sensor Node) and have another node (my board) with MC13224V rev 2.1 

 

The codebase in both are correct.

 

In the coordinator node i have 22 endpoints and in my board i have 16 endpoints. Well, i can bind key between boards and works fine. In both i receive BindSuccess and the led stop flashing.

But when i try to send a ASL_ZclOnOffReq from by board to coordinator board i can't. I receive the zbStatus_t with the value 0xA4 that can meaning gApsInvalidBinding_c or gZbInvalidEndpoint_c. The second value is not possible because the value of endpoint is correct (between 0x01 and 0xF0).

 

What I am doing wrong? Any suggestion would be appreciate....

 

Thanks

 

Added p/n to subject.

 

Message Edited by NLFSJ on 2009-06-02 09:16 AM
ラベル(1)
0 件の賞賛
返信
1 解決策
1,544件の閲覧回数
tpicon
Contributor II

Sorry everybody

I could see my error

 

My application (in both boards) can't register more than 4 endPoints...

 

Now, i need to understand why...

 

Regards

 

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,545件の閲覧回数
tpicon
Contributor II

Sorry everybody

I could see my error

 

My application (in both boards) can't register more than 4 endPoints...

 

Now, i need to understand why...

 

Regards

 

0 件の賞賛
返信