best way to initialize a TPM in PWM mode.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

best way to initialize a TPM in PWM mode.

4,067 Views
TurboBob
Contributor IV
I am using the TPM modules with the Processor Expert beans.  They work great, but when the cpu initializes, the output pin sends at least one pulse.  There is a pull-down on the output to be sure its low during initialization.
 
I have the PWM mode 'disabled' and initialized to 'low' in the bean.  Is there something I am missing?
 
Thanks
 
Bob
Labels (1)
0 Kudos
Reply
5 Replies

2,406 Views
ProcessorExpert
Senior Contributor III
We need more information in order to reproduce a problem. Could you please provide us a project demonstrating this problem or send us settings of PWM bean?

What version of Code Warrior and Processor Expert are you using?
Which derivative are you using?

best regards
Vojtech Filip
Processor Expert Support Team
UNIS
0 Kudos
Reply

2,406 Views
TurboBob
Contributor IV
can you give me an email address to send the file?

Its a JM60

Its codewarrior 6.2,  I will check the PE version and post it.


bob
0 Kudos
Reply

2,406 Views
TurboBob
Contributor IV
PE version is 3.03
 
Bean init is attached
 
 
0 Kudos
Reply

2,406 Views
ProcessorExpert
Senior Contributor III
I have not reproduced such behaviour therefore could you please send a project demonstrating the problem to: support(at)processorexpert.com

best regards
Vojtech Filip
Processor Expert Support Team
UNIS
0 Kudos
Reply

2,406 Views
TurboBob
Contributor IV
sent the project to you
 
thanks
 
 
0 Kudos
Reply