about s12vr64 AD Temperature

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

about s12vr64 AD Temperature

829件の閲覧回数
1073522577
Contributor I

I  want to ask about s12vr64  AD Temperature,  my  init  as follow.but the result of ADvalue isn't   correct.The channel  is   0x41,There was no significant difference at different temperatures.Can you tell me the solution?

void ADC_init(unsigned long BUS_CLK){
// ATD0TEST1 ATD0CTL2
/* Select 8-bit resolution*/
ATDCTL1_SRES =0;
/* Right justify data */
ATDCTL3_DJM = 1; // ATDCTL2
/* One conversion per sequence */
ATDCTL3_S1C = 1;
ATDCTL3_S2C = 0;
ATDCTL3_S4C = 0;
ATDCTL3_S8C = 0;
/* Select sample time 4 ATD clock cycles */
ATDCTL4_SMP = 0;
/*The temperature sensor and bandgap voltage amplifier is enabled.*/
CPMUHTCTL_HTE =1;
/* An internal temperature proportional voltag VeHT can be accessed internally */
CPMUHTCTL_VSEL =0;
/* ATD clock Prescaler */
ATDCTL4_PRS = (unsigned char) ((BUS_CLK/(2*ATD_CLK)) - 1);
}

0 件の賞賛
返信
0 返答(返信)