Zigbee: 13192 PLL lock?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Zigbee: 13192 PLL lock?

3,036件の閲覧回数
bshaw
Contributor III
What causes a lost lock interrupt on a MC13192? The manual states that it can happen but does not state what causes it or what to do to fix it. I'm getting this interrupt constantly while trying to do a CCA.

I'm using SMAC 4.0 on a mc9s08gt60 to talk to the mc13192. I'm getting through the '192 register initialization OK and reading back sane values from the '192. As soon as I try my first CCA I get the lost PLL lock interrupt.

Any thoughts would be appreciated, I'm stuck here.

Best,

Bill
ラベル(1)
0 件の賞賛
返信
2 返答(返信)

1,359件の閲覧回数
Ware
Contributor III

 

I always get this when the PHY layer interface is not correctly assigned...

I.E. wrong library or wrong definitions for Xcvr interface on custom hardware...  see "App_Target.h" and "Target.h"

 

Regards,

 - Ware

 

0 件の賞賛
返信

1,359件の閲覧回数
UK_CF_FAE
NXP Employee
NXP Employee
Hi Bill,
 
Is this your own hardware or a Freescale development board? Undoubtedly, the cause of the PLL losing lock is noise upsetting it.
 
Give us some more details, and we'll try to help.
 
Mark
0 件の賞賛
返信