ZStar3 data rate/sampling frequency

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

ZStar3 data rate/sampling frequency

1,920 次查看
radja
Contributor I

Dear Freescale Zstar team,

 

I am very interested in the Zstar3 Demo Board. The only thing stopping me from ordering it is the available sampling rates. Therefore I would like to ask if it is possible to raise the sampling frequency at least to 500 MHz. 

 

Thank you very much for your help

标签 (1)
0 项奖励
回复
1 回复

1,084 次查看
Gargy
NXP Employee
NXP Employee

Hello ,

 sorry but not at this version, because communication protocol (as is current version) doesn't count with higher datarate than 120Hz. Also used sensor are internally limited to cca 300Hz - so 500 Hz is needless know.

 

The 120Hz limitation was set as a compromise beetween speed and number of sensors.

It could be possible some future update that allows glue two rf time slots to one bigger and make datarate higher.

 

Have a nice day

 

0 项奖励
回复