Z-Stack in MC9S08GT32 is it possible?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Z-Stack in MC9S08GT32 is it possible?

2,495 Views
xevi
Contributor I
Hi,
I want to program a MC9S08GT32 with Z-stack and a simple application.
I don't know if 32kB of flash and 2kB of RAM is enought. 
I don't need to be ZigBee, but the hopping is interesting for me. I would use a tree topology(I thing the simplest). Is it possible?
 
Is it possible if the device was an end device in this type of topology?
Labels (1)
0 Kudos
Reply
1 Reply

1,351 Views
Mads
Contributor V
Hi Xevi,
using the GT32 is not possible. There is simply not enough flash, and ram for it.
Not even for an end device.
 
BR,
Mads
0 Kudos
Reply