Writing EEPROM does not appear to be persistent when using example AN4570. MC9SO8PA4

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Writing EEPROM does not appear to be persistent when using example AN4570. MC9SO8PA4

ソリューションへジャンプ
15,886件の閲覧回数
gregoryberardi
Contributor II

I am using the examples from AN4570. The example "EEPROM_ProgramUpto4Bytes". I am writing to location 0x3100 and the data is visible when using the "Memory Monitor" but when the chip is reset the data goes back to 0xFF.  I am erasing before writing and the functions are returning success. I am assuming that the BUSCLK is the 4MHz crystal that is clocking the chip (the datasheet is vague about this) so I have set FCLKDIV to 0x03 (3.6 to 4.6MHz). Any ideas on what I'm doing wrong?

ラベル(1)
タグ(3)
1 解決策
14,950件の閲覧回数
pavel_sadek
NXP Employee
NXP Employee

HI

Before command write sequence, NVM_FCLKDIV should be written to configure the flash clock to be between 0.8 and 1MHz.

be sure you are running the routine from RAM.

Pavel

元の投稿で解決策を見る

0 件の賞賛
返信
24 返答(返信)
3,104件の閲覧回数
zbeehu
Contributor II

I also ran this code on myPA4TWR board -

then,I also close the watchdog

when I debug,it also show  NO source available for"0x0000(0x0000)()"

0 件の賞賛
返信
3,101件の閲覧回数
gregoryberardi
Contributor II

I have been trying to run the code in ram but have run into a problem. When I uncomment the lines that copy flash to ram, the debugger fails to launch. I get the error shown in the attached image (EEPROM_ERROR_DEBUG.png).

I am attaching the project that is giving me the issues. The copy lines are in the file hal_eeprom_init.c. Lines 58 and 60.

The chip that I'm running this on is a MC9S08PA4. There is only 512 bytes of ram. The two functions (erase and write) are a total of 204 bytes. I am left with a very small amount of RAM. Could I use the same ram space and copy the functions in as I need them?

Thank you in advance!

0 件の賞賛
返信
3,101件の閲覧回数
gregoryberardi
Contributor II

I have not been able to try running from ram but I believe that was my issue.

Thank you all!

14,951件の閲覧回数
pavel_sadek
NXP Employee
NXP Employee

HI

Before command write sequence, NVM_FCLKDIV should be written to configure the flash clock to be between 0.8 and 1MHz.

be sure you are running the routine from RAM.

Pavel

0 件の賞賛
返信