Why STOP mode can execute once only in MC9RS08KA2?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Why STOP mode can execute once only in MC9RS08KA2?

1,765件の閲覧回数
JohnFM
Contributor II
I want my MC9RS08KA2 to go to STOP mode, get out by KBI, do something and loop bak to STOP mode again continuously.
I configured my MCU so that it went to STOP mode and was taken out by KBI. Everything was fine the first time STOP instruction was executed, i.e. it really stopped there at the STOP instruction, when there is a KBI, it continued with the next instruction. However, if I let it execute another STOP instruction after successfully getting out (by KBI), the second STOP instruction was ignored, i.e. it didn't stop there at this second STOP instruction but immediately continued with the next instruction. Could someone tell me why?
 
John
ラベル(1)
0 件の賞賛
返信
2 返答(返信)

858件の閲覧回数
BasePointer
Contributor II
I think you can't handle keyboard interrupt properly. Show your interrupt handler.
Be sure that KBI interrupt flag was cleared before stop instruction.
0 件の賞賛
返信

858件の閲覧回数
JohnFM
Contributor II
Yes, it works now by clearing KBI interrupt flag. Thanks a lot!
0 件の賞賛
返信