What program (work in Win2k) can work with my circuit to load flash to MC68HC908JB8 ?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

What program (work in Win2k) can work with my circuit to load flash to MC68HC908JB8 ?

3,001 Views
quangpk
Contributor I
Pls, introduce to me what program (work in Win2k) can work with my circuit to load flash to MC68HC908JB8,
Best Regards,
 
Message Edited by t.dowe on 2009-09-16 10:08 AM
Labels (1)
0 Kudos
Reply
4 Replies

1,312 Views
erooll
Contributor II
Hi.
If you need IDE enviroment to develope, i suggest use CodeWarrior, this also allow program trought a MON08 interface that is that you shows.
If you only need program flash maybe PROG08 programmer software (from P&E) could be util
Regards.
0 Kudos
Reply

1,312 Views
quangpk
Contributor I
- Yes, I use CodeWarrior 6.1
- Can you give me link to download PROG08 from P&E, this proggram can comm with my circuit through RS232 interface ?
Quang,
0 Kudos
Reply

1,312 Views
peg
Senior Contributor IV
Hi quangpk,

If you have CW then you basically have this included, but here is the link anyway.
You will have to sign up to get access to it.

0 Kudos
Reply

1,312 Views
fjrg76
Contributor IV
Have you tried CodeWarrior??
0 Kudos
Reply