What program (work in Win2k) can work with my circuit to load flash to MC68HC908JB8 ?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

What program (work in Win2k) can work with my circuit to load flash to MC68HC908JB8 ?

3,006 次查看
quangpk
Contributor I
Pls, introduce to me what program (work in Win2k) can work with my circuit to load flash to MC68HC908JB8,
Best Regards,
 
Message Edited by t.dowe on 2009-09-16 10:08 AM
标签 (1)
0 项奖励
回复
4 回复数

1,317 次查看
erooll
Contributor II
Hi.
If you need IDE enviroment to develope, i suggest use CodeWarrior, this also allow program trought a MON08 interface that is that you shows.
If you only need program flash maybe PROG08 programmer software (from P&E) could be util
Regards.
0 项奖励
回复

1,317 次查看
quangpk
Contributor I
- Yes, I use CodeWarrior 6.1
- Can you give me link to download PROG08 from P&E, this proggram can comm with my circuit through RS232 interface ?
Quang,
0 项奖励
回复

1,317 次查看
peg
Senior Contributor IV
Hi quangpk,

If you have CW then you basically have this included, but here is the link anyway.
You will have to sign up to get access to it.

0 项奖励
回复

1,317 次查看
fjrg76
Contributor IV
Have you tried CodeWarrior??
0 项奖励
回复