What does Error 14 mean? - MC13213

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

What does Error 14 mean? - MC13213

2,374件の閲覧回数
VincentLau
Contributor I
Hi, all
 
   What does error 14 mean when I trying to download code into my PCB for MC13213 though PE?  I measure the reset signal, there is a regular disturb peak signal in it. And there is no signal output on CLK0. Why it happen? Can anyone help me?
 
Best Regards
 
Vincent
July 15, 2008
 
 
 
 
Added p/n to subject.


Message Edited by NLFSJ on 2008-07-15 08:35 AM
ラベル(1)
0 件の賞賛
返信
2 返答(返信)

1,387件の閲覧回数
Zahar
Contributor IV
Hello Vincent,

A pulse on a RESET line means that your processor is always resetting.

Error 14 on the other hand means that there is a problem with loading the algorithm.

What is the name and the version number of P&E software that you are using? Please attach an algorithm that you are using to this message thread.

What is the name/revision of the hardware interface that you are using?

Are you using an evaluation board from Freescale, or is this a custom board of your own design?

Best Regards,
Zahar
P&E
0 件の賞賛
返信

1,387件の閲覧回数
peg
Senior Contributor IV
Hi
Those pulses on reset are normal.
Refer to this thread.

0 件の賞賛
返信