Using USB Multilink MON08 for HC908GP32

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Using USB Multilink MON08 for HC908GP32

1,589 Views
mylim
Contributor IV

Hi, I am having some problem entering debugging mode using MON08 on GP32 but I manage to do it for AB32.

Can Anyone give any advise?

I have also attached some pictures of my PCB debug pin connection and my mon08 connection pictures.

Please advise.

Thanks.

 

Regards,

MY

Labels (1)
0 Kudos
Reply
1 Reply

1,326 Views
PeterHouse
Contributor I

MY,

 

It has been awhile since I made a MON08 interface for a GP32.  As I recall there are 3 pins which must be in the correct state when the reset pin goes inactive.  These pins specify the baud rate, baud rate source, and boot mode of the GP32.  If the boot mode is MON08 then the GP32 will be available to connect serially using pin PTA0 to your MON08 host and receive commands.

 

I found a schematic of a GP32 production board I made and attached it to this response.  As you can see, when the CPU08 programmer is attached, the PA7 and PC1 pins are pulled low and the PC0 and PC3 pins are pulled high. 

 

In production none of the diodes were stuffed and a bed of nails fixture was used for program and test.

 

Good Luck,

 

Peter

 

0 Kudos
Reply