Using S08AW16, Bus clock is 16MHz, watchdog time too short. Is there a solution?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Using S08AW16, Bus clock is 16MHz, watchdog time too short. Is there a solution?

Jump to solution
2,506 Views
w_tension
Contributor III

Only 2^13 or 2^18 modes. Max time = 16M / 262144 = 16.4ms.

I know maybe it's hopeless.

Tags (2)
0 Kudos
Reply
1 Solution
2,384 Views
vicentegomez
NXP TechSupport
NXP TechSupport

Hi

Yes, the watchdog only has two timers 2^13 or 2^18, but also you can disable it. 

But I do not know what is your application where you need a long watchdog timer, do you plan to have more than 17 ms on the same task that you can not feed the dog.

Regards

View solution in original post

0 Kudos
Reply
2 Replies
2,385 Views
vicentegomez
NXP TechSupport
NXP TechSupport

Hi

Yes, the watchdog only has two timers 2^13 or 2^18, but also you can disable it. 

But I do not know what is your application where you need a long watchdog timer, do you plan to have more than 17 ms on the same task that you can not feed the dog.

Regards

0 Kudos
Reply
2,384 Views
w_tension
Contributor III

Thanks for your answer.

Long time can simplify coding.

Otherwise, I need feed the watchdog every where. For example: SCI transmit SPI transceiver and time delay.

0 Kudos
Reply