Using GPIO on PC9RS08LE4

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Using GPIO on PC9RS08LE4

Jump to solution
2,081 Views
Darkn3ss
Contributor II

Hello all.

 

Here is the deal.

 

My Vcc is 5V from a 7805 regulator.  I am using a few PC9RS08LE4 samples from Freescale.

 

The code is as follows:

    PTDDD = 0xFF;
    PTDD = 0xFF;

 

What voltage should my 8 port pins be for the output?  The datasheet says Vdd-0.8 is Voh, and 0.8V is Vol, but I am getting 0V low, and only 0.3V when they are all on.

 

I've thought that perhaps the LCD functionality was on, but checking the value of LCDC0 in the debugger, it actually is set to 0x03 (the value after reset).  I tried resetting it to     LCDC0 = 0x00; but no luck.

 

Has anyone had any luck with this part using the LCD pins as GPIO?  I'm certainly missing something here, but I have no idea what it could be.

 

Thank you in advance for any help that can be provided!  :smileyvery-happy:

Labels (1)
0 Kudos
Reply
1 Solution
1,710 Views
Darkn3ss
Contributor II

SOLUTION!

 

Apparently there is an error in my interpretation of the documentation, or the documentation itself.

 

If you turn the LCD off, I would think that a GPIO is a GPIO.  This is not the case.

 

LCDSUPPLY needs to have VLL3 driven externally.  What this means?  I don't know.  Anyways, set LCDSUPPLY = 3;

Then, LCDC1 = 0x03; sets up the GPIO pins shared with the LCD pins to be used as a full complimentary output, instead of an open drain output.  I figured this out luckily because I decided to re-wire one of my NPN transistors with a PNP and totem-pole them for a redundant circuit, and turning on the PNP worked like a charm!  Well, not I know why!  Searched open drain in the RM, and I found this gem.

 

Good luck to anyone else that comes across this!  I hope my solution will help you some.

View solution in original post

0 Kudos
Reply
1 Reply
1,710 Views
Darkn3ss
Contributor II

SOLUTION!

 

Apparently there is an error in my interpretation of the documentation, or the documentation itself.

 

If you turn the LCD off, I would think that a GPIO is a GPIO.  This is not the case.

 

LCDSUPPLY needs to have VLL3 driven externally.  What this means?  I don't know.  Anyways, set LCDSUPPLY = 3;

Then, LCDC1 = 0x03; sets up the GPIO pins shared with the LCD pins to be used as a full complimentary output, instead of an open drain output.  I figured this out luckily because I decided to re-wire one of my NPN transistors with a PNP and totem-pole them for a redundant circuit, and turning on the PNP worked like a charm!  Well, not I know why!  Searched open drain in the RM, and I found this gem.

 

Good luck to anyone else that comes across this!  I hope my solution will help you some.

0 Kudos
Reply