Unused INT trap. RTI or send to start of prog?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Unused INT trap. RTI or send to start of prog?

1,672件の閲覧回数
JimDandy
Contributor III

I'm using an 'HC908JK3 in a noisy automotive ignition environment. Have several variations on a theme over half a dozen different boards, the relevant code being virtually identical except for I/O differences to help board layout. One board in particular has a habit of acting up for some customers although I have not been able to reproduce it on the bench. My recent post regarding what to do with unbonded input pins was a big help in getting on top of this problem, so thanks to all that helped.

 

Anyway, my code uses no interrupts so I want to put a trap in the vector area so if a spurious interrupt does occur it can recover gracefully. What is the best way of doing this? I have all interrupts disabled but I want to go both belt and braces.

 

               ORG     $FFDE

               RTI

               ORG     $FFE0

               RTI

               etc,

 

OR

 

               ORG     $FFDE

               FDB     START

               ORG     $FFE0

               FDB     START

               etc

 

"START" is the very top of the listing, the reset vector.

 

Regards,

Graham

ラベル(1)
タグ(4)
0 件の賞賛
返信
4 返答(返信)

1,508件の閲覧回数
Monica
Senior Contributor III

Hello Graham,

has this worked out for you? Please let us know if the suggestions were helpful, we'd like to hear.

Best regards,

Monica.

0 件の賞賛
返信

1,508件の閲覧回数
JimDandy
Contributor III

Hello Monica,

Unfortunately, no, it has not fixed my problem yet. My code is certainly more airtight now though. We are going to make a fairly comprehensive test setup in the next few weeks hopefully so we can reproduce the problem and then try a few different approaches. Till then I just have to wait.

Regards,

Graham.

0 件の賞賛
返信

1,508件の閲覧回数
bigmac
Specialist III

Hello Graham,

Exiting a spurious interrupt as quickly as possible is probably the best approach, unless the noise burst that caused the interrupt has additionally corrupted registers, etc.  In this instance you may wish to force a reset, perhaps by purposely generating an illegal operation ILOP error reset.  You will need to judge which would be the least disruptive to normal operation.

Placing a RTI instruction at each vector location will not work - the interrupt is entered by fetching the address present at the vector location.  So the following approach would be needed.  You may also wish to consider placing additional diagnostic code within the ISR, so that the number of spurious interrupts that occur  may be interrogated in some manner.

ILOP  equ   $3E

DUMMY_ISR2:  ; Causes illegal operation reset

      ILOP

DUMMY_ISR1:  ; Exit interrupt

      rti

...

; Vector table:

  org $FFDE

      fdb  DUMMY_ISR1  ; ADC conversion

      fdb  DUMMY_ISR1  ; Keyboard

  org $FFF2

      fdb  DUMMY_ISR1  ; TIM overflow

      fdb  DUMMY_ISR1  ; TIM channel 1

      fdb  DUMMY_ISR1  ; TIM channel 0

      fdb  $FFFF       ; Not used

      fdb  DUMMY_ISR1  ; IRQ

      fdb  DUMMY_ISR1  ; SWI instruction

      fdb  START       ; Reset

It may also be possible that the noise burst is corrupting the I/O setup.  In particular the data direction and pull-up enable registers may be critical to operation.  Traditionally, these registers are initialised following a reset, and are then expected to remain uncorrupted for an indefinite period, maybe days, weeks or months in some instances.  You may therefore find that it be desireable to re-initialise the data direction and pull-up enable registers on each circuit of the main loop.

Regards,

Mac

0 件の賞賛
返信

1,508件の閲覧回数
Derrick
NXP Employee
NXP Employee

The problem with the "DUMMY_ISR1" approach is that it does not clear the source of the interrupt request.  For example, if the source of the interupt was TIM Channel 0 then you will need to clear the timer interrupt flag before issuing the RTI instruction - i.e., TSC0[CH0F].  If you don't clear this flag the interrupt is still pending and you will simply thrash back and forth into and out of the DUMMY_ISR1 routine forever - or until the watchdog resets you.

Since you're not using interrupts, you could enhance the DUMMY_ISR1 routine such that it clears all interrupt request flags from all peripherals:

DUMMY_ISR1:

        bset    ACK,INTSCR      ; clear IRQ pin request

        bclr    TOF,TSC         ; clear TIM overflow request

        bclr    CH0F,TSC0       ; clear TIM Channel 0 request

        bclr    CH1F,TSC1       ; clear TIM Channel 1 request

        bset    ACKK,KBSCR      ; clear Keyboard request

        rti

I would also suggest assigning all interrupt vector locations (i.e., from $FFDE to $FFFD), whether they are used or not.

Best Regards,

Derrick

0 件の賞賛
返信