Unknown Base plugin Nub error

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Unknown Base plugin Nub error

3,565 Views
tcherno
Contributor II

hello,

I have a project in Code Warrior 10.6.4 IDE developed for MC9S08QE128 MCU.

I am using PE micro Multilink FX as a debugger and programmer.

 

until a week ago I was able to debug and burn the code. to the flash of the MCU with no problem.

now when i try to debug or burn the code i get the error "Unknown Base Plugin Nub error".

 

with the PROGHCS08 - Flash Programmer Software from PE micro i have no problem burning the code on the board with the same debugger.

 
when checking the signal of the BDM, i can see that the PC tried to initiate connection with the MCU.

 

have anyone faced this problem and can help me?

 

thank you,

omer

2 Replies

3,479 Views
pawantanwar
Contributor I

Restart CodeWarrior and reconnect the Multilink FX. Update P&E drivers for CodeWarrior and Multilink FX. Reset debug settings (Project > Properties > Debug/Launch Settings) and clear the workspace cache by deleting the .metadata folder.

thanks and regards
pawantanwar
https://www.multispanindia.com



 

3,534 Views
Pablo_Ramos
NXP Employee
NXP Employee

Hi @tcherno,

I noticed that you already made a similar question on other community post. There is some activity in said post so please follow up there. I’m adding a link here for reference of other community users that may find it helpful.

Unknown Base Plugin Nub error - NXP Community