USBSPYDER08 driver

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

USBSPYDER08 driver

2,179 Views
Blaise34
Contributor I

Hi,

 

I havent used my USBSPYDER08 for a while, but now I would like to  use it again.

Unfortunately I can not find the installation CD for it.

 

Can someone help me to find this driver somewhere?

Will it work on a 64 bit Vista, or should I use my old machine with 32 bit XP?

 

The latest CW SE (10.01 Eclipse based) still supports USBSPYDER? Probably the Classic one?

 

Thanks for your kind help in advance.

 

Best regards,

Laszlo

Labels (1)
0 Kudos
Reply
1 Reply

1,432 Views
Blaise34
Contributor I

Hi,


I'm answering my questions then.


- The Softec driver for USBSPYDER08 can be found on the Internet. You should search for the file name usbspyder08_setup.exe.


- No, this driver does not work on 64 bits OSes. I have tryed the WinUSB driver with the Spyder but I have no success.


- No, the Eclipse based CW seems not to work with Spyder, however if you chose the OSBDM interface and then select Softec the Spyder is listed. Anyway I was not able to make it working.


- The Classic version of CW (6.3) is supporting the Spyder interface and it is working fine. Please note that this version of CW can not be installed on 64 bits OSes.


Best regards,

Laszlo

0 Kudos
Reply