USB vs PARALLEL MON08 MULTILINK and In-Circuit Simulator

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

USB vs PARALLEL MON08 MULTILINK and In-Circuit Simulator

2,600 Views
girmauro
Contributor I
Hi,
we've used always the MON08 MULTILINK with parallel port with our MC68HC908GP32 micro and WinIDE development tool; we always debug our code with In-Circuit Simulator (code run in RAM, doesn't?) and only at the end we program flash.
Recently we've buy an USB MON08 multilink debugger-programmer and try to do the same, but the in-circuit simulator not recognize the usb-port. It works only if we first program flash and then run In-Circuit Debugger, but time of debugging is too long; what's the problem?
Thanks
girmauro
Labels (1)
0 Kudos
Reply
2 Replies

1,616 Views
Zahar
Contributor IV
Girmauro,

What revision of USB ML MON08 are you using? What is the firmware version number?

You have to make sure that you are using the latest P&E software.

Please submit a support request here: http://www.pemicro.com/SRS/main_screen_user.cfm

We will then provide you with the latest software that we probably solve your problem.

Best Regards,
Zahar
P&E


0 Kudos
Reply

1,616 Views
JimDon
Senior Contributor III
I'd run this by P&E support they are very good and should answer your question quickly.
0 Kudos
Reply