USB Interface in MC9S08JM16

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

USB Interface in MC9S08JM16

3,334 Views
Archer
Contributor I
Hi,

How to change the class in USB module,
I want to use TMC,
but when i read the AN3565 about CMX USB stack, there is onlt cdc and HID class.
I am newbie in this IC,

Thanks a lot.

Archer Chang
Labels (1)
0 Kudos
Reply
3 Replies

1,945 Views
sailor
Contributor I
Dear sir,
     I use the CMX_USB_LITE_ to do my project, The MCU is MC9S08JM16. I use the Virtual serial port of the stack.Sometimes the Virtual serial port is not stable.
I want to re-enumeration the device when the Virtual serial port is not stable,but  i don not know how to do in Programm,Please give me your advice.
 
Best Regards!
0 Kudos
Reply

1,945 Views
Goz
Contributor I
The CMX stack supplied does not support the TMC class. You will find that there aren't many vendors that do support TMC, so you are on your own a bit with this one.
You may just have to do a bit of a search of the web to see if anyone has some open source code available for the TMC class.
0 Kudos
Reply

1,945 Views
baja_usb
Contributor II

Hi Archer, did you secceded? I'm trying to write a TMC driver but on the Medical USB Stack on a MCF51JM128

 

Regards,

Daniel

0 Kudos
Reply