USB Communication

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

USB Communication

2,698 次查看
OualBel
Contributor I

Hello,

 

I have a card with S08JM60 Freescale microcontroller.

I have established a USB communication between my card and a Host PC.

 

Know, i neeed to add some code lines in order to give an information

when USB communication is not established

 

Thanks

标签 (1)
0 项奖励
回复
3 回复数

2,399 次查看
Tsuneo
Contributor IV

Sound like a self-powered device.

Assign a port pin to detect VBUS (5V) voltage at the USB connector.

 

Tsuneo

0 项奖励
回复

2,399 次查看
OualBel
Contributor I

Hello,

 

I have a Card connected with an USB2.0 connector to a MotherBoard with an I3 processor.
My Card is realized around the S08JM60 Microcontroller.
Sometimes, the my card is not recognized by the Motherboard with the I3 processor.
I need to know, how can i detect, if my Card is connected or not connected?
Exactly, in which part in the Source code USB of the microcontroller S08 ?

 

Best regards

0 项奖励
回复

2,399 次查看
Tsuneo
Contributor IV

Continue in your another post.

https://community.freescale.com/thread/96766

 

Tsuneo

0 项奖励
回复