UART bootloader for MCF51QE

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

UART bootloader for MCF51QE

4,579件の閲覧回数
sarmassi
Contributor II

HI,

I'm interested about BOOTLOADER, I have developed my application for mcf51qe128.

Until today i have downloaded the fw with cyclone. Now there is a need to download with the UART.

I have a .pdf  "Implement UART Boot-loader On Coldfire V1 Products" written by Paol Zhang, but I haven't the project of him. Where can I find that? Thank you

ラベル(1)
タグ(1)
6 返答(返信)

4,357件の閲覧回数
markdonkers
Contributor I

Thank you Vincente!

The files that you sent are related to AN2295. I was actually more interested in the files that support the PDF by Paul Zhang titled, Implement UART Boot-loader On Coldfire V1 Products. The document can be found here:

http://read.pudn.com/downloads132/sourcecode/embed/561869/Implement%20UART%20Bootloader%20On%20CF%20... 

I

Regards,

Mark

0 件の賞賛
返信

4,357件の閲覧回数
vicentegomez
NXP TechSupport
NXP TechSupport

Yes, I saw that document, the problem is that the software is not available, but I know that Paul based on the an2295.

regards

Vicente 

0 件の賞賛
返信

4,357件の閲覧回数
vicentegomez
NXP TechSupport
NXP TechSupport

I will send you the file through email

regards

4,357件の閲覧回数
markdonkers
Contributor I

Hello. I am also in need of the actual project. Could you either of you also send it to me too? Perhaps it would make sense to also attach it to this thread.

Thanks,

Mark

0 件の賞賛
返信

4,357件の閲覧回数
vicentegomez
NXP TechSupport
NXP TechSupport

I have send you the an2295sw with the qe family

0 件の賞賛
返信

4,357件の閲覧回数
sarmassi
Contributor II

thank you very much

0 件の賞賛
返信