Trouble with drivers for demoqe128

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Trouble with drivers for demoqe128

1,902 次查看
irenemlc
Contributor I

Hello, I recently bought a Demoqe128 and it works perfectly on my Win7 64 bits PC. I only installed CW10.3, connected the device and didn't have a single driver issue.

 

The problem is with the Win7 32 bits partition of my Macbook, I installed  CW10.3 with the same archive I used on my PC, but when I connect the device the laptop says it cannot find the Serial and Debug drivers, i tried with the troubleshooting and it couldn't find them online, I used Instdrivers and DPinst and it said that all drivers had been installed, but when i reconnected the device the problem remained.

 

The only thing I haven't done is installing another version of Windows, but I don't see how that would help, I suppose it's the Mac's fault.

 

I really need to get this working for college, so I would appreciate any help or ideas you could give me.

 

Thanks in advance.

 

 

Images of the problem in question:

4501_4501.PNGerror1.PNG

 

4505_4505.PNGerror2.PNG

标签 (1)
0 项奖励
回复
3 回复数

1,740 次查看
Joel69003
Contributor IV

Hi Irene,

Sure you don't have the right drivers. I don't know which king of debugging cable is used on your demo board, but it is probably something similar to the Multilink cable : P&E Microcomputer Systems - USB BDM Multilink Cable - USB BDM Interface cable for the <b&...

1/ Have you got some drivers delivered with the board ? If yes try installing those drivers throw the Device Manager.

2/ If you don't have any drivers, you can get P&E Multilink drivers at the previous link. Download and try to install. Note that you will have to register.

Let known if it works after that.

Regards,

Joel Guittet

1,740 次查看
irenemlc
Contributor I

Hello, I tried with the drivers but it didn't work so I uninstalled and installed it a couple times until the laptop recognized the drivers during the installation. I still don't know what the problem was but it seems to be working now.

Thank you for helping me out.

0 项奖励
回复

1,740 次查看
Joel69003
Contributor IV

Nice to know you have solved the issue :-)

Joel

0 项奖励
回复