Trigger A & B occurred??

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Trigger A & B occurred??

4,361 Views
HarrySun
Contributor I
in CW debugger, it sometime shows "Trigger A & B occurred"
what does it mean??
thanks

 
Labels (1)
0 Kudos
Reply
3 Replies

1,904 Views
YeOldeBDM
Contributor III
I have seen this message when the power on the target is interrupted, or the bdm connection is intermittent.
0 Kudos
Reply

1,904 Views
CrasyCat
Specialist III
Hello
 
That message is generated when you have enabled some triggers on the DBG module.
In the connection menu (MultilinkCyclonePro, GDI, .....) select "Trigger Module Settings".
 
There are probably some triggers defined in the Trigger settings tab.
Delete the triggers if you do not want to see the message again.
 
CrasyCat
0 Kudos
Reply

1,904 Views
joerg
Contributor II
Hi
or you have triggered an interrupt but the vector setting is not correct! I.E. there was an TIM OC interrupt but you have forgoten to set the VECTOR x (in the prm file) to your interrupt routine.

Saluti Joerg
0 Kudos
Reply