Timer and sleep behavior: debugger vs no debugger

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Timer and sleep behavior: debugger vs no debugger

1,287 Views
matthammond
Contributor I

On the MC13234, I'm seeing some weird inconsistencies in timer and sleep behavior between when I download the code and have the debugger attached, and when the debugger is not attached and the code is running freely. I'm interested if anyone could give me some tips or point me toward an application note that explains the differences in how the timers and STOP3 mode might work with and without the debugger attached, so I can track down the source of the discrepancy and find a workaround.

Thanks!

Labels (1)
0 Kudos
Reply
0 Replies