The Classification and Application of Microcontrollers

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

The Classification and Application of Microcontrollers

1,530 次查看
xiaoye
Contributor I

Microcontrollers are classified into two types based on their memory type: those with no on-chip ROM  and those with on-chip ROM,  The chip without on-chip ROM  must be used externally with EPROM (typically 8031); the chip with on-chip ROM  is classified as on-chip EPROM (typically 87C51), MASK on-chip mask ROM  (typically 8051), on-chip Flash (typically 89C51), and other types.

MCUs are classified into two types based on their intended use: general-purpose and special-purpose. It is classified into4, 8, 16, and 32-bit MCUs based on the width of the data bus and the number of data bytes that can be processed at the same time.

0 项奖励
回复
0 回复数