TWR=MCF51CN Bootloader Mode problem

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

TWR=MCF51CN Bootloader Mode problem

1,524 Views
pawelniewiadoms
Contributor I

Hello,

I have TWR-MCF51CN board and I have problem with bootloader mode in it. When I want to update my firmware by P&E firmware updater I have to use jumper on J16. When I've done it my device become undetected. When I use CodeWarrior v10.6.4 it also makes update of my firmware and it's the same problem. It happens when I reconnect my board with jumper on. Without jumper on J16 my device is detected. I'm using Mini USB cable as debugger.

Thanks for all responses.

Greetings,

Pawel.

Labels (1)
0 Kudos
Reply
1 Reply

1,403 Views
vicentegomez
NXP TechSupport
NXP TechSupport

Hi Pawel

The J16 is only use if you want to update the firmware on the JM60 (OSBDM), if this is present you only can update the firmware with the P&E tools.

If you want to program the MCF51CN you need to remove the J16.

Regards

Vicente Gomez

0 Kudos
Reply