TPM1MOD PWM abnormal

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

TPM1MOD PWM abnormal

2,868 Views
konstantinoshal
Contributor I

Hello,

 

In one of our products we use the MC9S08SE4 microcontroller.

We have noticed that when we change the PWM period (TPM1MOD) in the timer overflow interrupt (Vtpm1ovf),

there are two PWM periods until next overflow interrupt.

 

Our code sample - in order to reproduce this issue - is:

 

unsigned int TPM1MOD_BUF;

 

void main(void)

{

    TPM1MOD = 500;

    TPM1CNTH = 0;

    TPM1C0SC = 0x28;

    TPM1C0V = 250;

    TPM1SC = 0x4B;

 

 

    EnableInterrupts;

 

 

    for(;;)

    {

        __RESET_WATCHDOG();

    }

 

}

 

interrupt VectorNumber_Vtpm1ovf void isr_Vtpm1ovf(void)

{

   

    TPM1SC;

    TPM1SC_TOF = 0;

    TPM1MOD_BUF = TPM1MOD;

    TPM1MOD_BUF += 100;

    TPM1MOD = TPM1MOD_BUF;

    TPM1MOD_BUF >>= 1;

    TPM1C0V = TPM1MOD_BUF;

    TPM1C1V = TPM1MOD_BUF;

 

}

 

Do you know why is this happening?

 

Thanks in advance.

Labels (1)
0 Kudos
Reply
4 Replies

2,379 Views
weapon
Senior Contributor I

Hi, That is normal behavior.

Please check the below mechanism of writing TPMxMOD, you can find it in the section 13.4.3 of  the reference manual (page 197)

Writing to either byte (TPMxMODH or TPMxMODL) latches the value into a buffer and the registers are

updated with the value of their write buffer according to the value of CLKSB:CLKSA bits, so:

• If (CLKSB:CLKSA = 0:0), then the registers are updated when the second byte is written

• If (CLKSB:CLKSA not = 0:0), then the registers are updated after both bytes were written, and the

TPM counter changes from (TPMxMODH:TPMxMODL - 1) to (TPMxMODH:TPMxMODL). If

the TPM counter is a free-running counter, the update is made when the TPM counter changes from

0xFFFE to 0xFFFF

If you turn off the TPM in the interrupt, then write TPMxMOD, the value will be updated immediately.

B.R

XWP

0 Kudos
Reply

2,379 Views
konstantinoshal
Contributor I

Dear Xu,

By using the exact same code to the MC9S08PA4 microcontroller, there is only one PWM period until next overflow interrupt.

According to the MC9S08PA4 datasheet - section 12.4.8.1 - the mechanism of writing TPMxMOD is the same. The only difference is that

the update is made when the TPM counter changes from 0xFFFF to 0x0000.


So, why there is different behavior on the two families?

Thanks,

Konstantinos.

0 Kudos
Reply

2,379 Views
weapon
Senior Contributor I

Hi Konstantinos,

The modules in S08SE and S08PA are different, but now I suppose I misunderstood the issue you met in S08SE. I just do some test in S08P family,

below is the code.

void FTM0_Init(void)

{

    FTM0_SC = 0;

    FTM0_C0SC = 0;

    FTM0_C1SC = 0;

    FTM0_MOD = 0xFFFF;

    PORT_PTDIE_PTDIE6 = 0;

    PORT_PTDOE_PTDOE6 = 1;

     

    PORT_PTDD_PTDD6 = 0;

   

     FTM0_SC = 0x4C; // start

}

// Interrupt Service Routine

ISR(IsrFTM0OVF)

{

// NOTE: The routine should include actions to clear the appropriate

//      interrupt flags.

//

    static byte overflow_count = 0;

    byte dummy;

  

    dummy = FTM0_SC;

    FTM0_SC_TOF = 0;

  

    FTM0_MOD = 0x5000;

  

    overflow_count++;

    if(overflow_count == 6)

    {

      

    }

    if(overflow_count == 12)

    {

        FTM0_SC_CLKS = 0;

    }

    PORT_PTDIE_PTDIE6 = 0;

    PORT_PTDOE_PTDOE6 = 1;

    PORT_PTDD_PTDD6 ^= 1;

}

In the ISR, I toggled one GPIO to be monitored by  an Osilloscope.  I got below waveform:

tek00000.png

We can see the first period is still 0xFFFF, and FTMxMOD is updated at the first falling edge(the second overflow interrupt).  

Is that what you observed in S08PA?  Could you share the waveform got from S08SE?

0 Kudos
Reply

2,379 Views
konstantinoshal
Contributor I

Dear Xu,

Please run the following example to a MC9S08SE4 controller. You should see the results as per attached images.

void main(void)

{

    PTAD = 0x00;

    PTADD = 0xFF;

    ICSTRM = 0xb9;

    ICSC2 = 0x00;

    TPM1CNTH = 0;

    TPM1MOD = 500;

    TPM1C0SC = 0x28;

    TPM1C0V = 250;

    TPM1SC = 0x4B;

  

    EnableInterrupts;

    for(;;)

    {

        __RESET_WATCHDOG();

    }

}

interrupt VectorNumber_Vtpm1ovf void isr_Vtpm1ovf(void)

{

     static unsigned int TPM1MOD_BUF;

     static unsigned char i;

     TPM1SC;

     TPM1SC_TOF = 0;

     TPM1MOD_BUF = TPM1MOD;

     TPM1MOD_BUF += 100;

     TPM1MOD = TPM1MOD_BUF;

     TPM1MOD_BUF >>= 1;

     TPM1C0V = TPM1MOD_BUF;

  

    if (++i == 4)

        TPM1SC = 0;

}

As you can see, between overflow interrupts, there are two periods. Notice, that in overflow interrupt the PWM

period is changing by altering the TPM1MOD register. The initial period is 500 usec and in each overflow interrupt

is increasing by 100 usec. So, the expected values would be: 500 -> 600 -> 700 -> 800 usec. Instead we see that

the output periods are: 500 -> 600 -> 600 -> 700 -> 700 -> 800 etc.

screenshot.pngscreenshot1.pngscreenshot2.pngscreenshot3.pngscreenshot4.pngscreenshot5.png

I hope everything is clear now.

Do you think that this is an abnormal behavior?

Thanks,

Konstantinos.

0 Kudos
Reply