Suggestion

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Suggestion

1,476 Views
Cn
Contributor I

Hello Forum

 

This is my first time using microcontrolers...

 

I'm looking a microcontroler with 8 i/o digital and also i want to read 8 analog signals (the range of
the signals it's arround 0-10 VDC) . And also i want to transmit my analog data to my computer using rs232

 

 
The project will be a prototype of Accelerate Life testing to DC motors, the spec of the motors it's 12 VDC @ 100 mA.
Could you suggest me any microcontroler
Thanks 
Labels (1)
0 Kudos
Reply
1 Reply

1,226 Views
Lundin
Senior Contributor IV

Pretty much any S08 will have what you need, such as the S08Q family. Consider what logic supply voltage you want before picking one though, some S08 only support 3V3 while some support 3V - 5V.

0 Kudos
Reply