Sorce code and Doc for BUFFALO or other Monitor  for 68HC11

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Sorce code and Doc for BUFFALO or other Monitor  for 68HC11

9,316 次查看
IrajRafiei
Contributor I
Hello everybody
 
 Could everyone help me find sorce code and doc for BUFFALO or other Monitor  for 68HC11?
 
Special Thanks
I. Rafiei
标签 (1)
0 项奖励
回复
4 回复数

2,572 次查看
jkenney3
NXP Employee
NXP Employee

Iraj,

Here is the BUFFALO assembly file.

Jim Kenney

 

buf34.asm

Message Edited by t.dowe on 2009-10-20 01:46 PM
0 项奖励
回复

2,572 次查看
jkenney3
NXP Employee
NXP Employee

Iraj,

The S19 file. I changed the extension to .txt so that the system would take it.

Jim Kenney

 

BUF34.txt

Message Edited by t.dowe on 2009-10-20 01:47 PM
0 项奖励
回复

2,572 次查看
Alban
Senior Contributor II
Hi Jim,
 
From now S19 and S2 are authorized on all boards. Thanks for flagging this up.
 
Alban.
0 项奖励
回复

2,572 次查看
jkenney3
NXP Employee
NXP Employee

Iraj,

 

I was looking for something else when I stumbled across your e-mail.  I looked thru my archives and found the attached files.  The User Manual is for the HC11EVB, a low cost evalutation board offered in the mid to late 90's.  It came with BUFFALO (Bit User's Fast Friendly Aid to Logical Operation) in the EPROM.  The UM can be considered a BUFFALO user's manual as well.  I have also attached the assembly code and S19 file for ver 3.4. (Looks like the message board allows only one attachment at a time.  I will send the code seperately.)

These come with no warranty of any kind.  You may need to dust them off before you use them as they have been on my shelf since 2000.

Have fun!

Jim Kenney

 

11evbu.pdf

Message Edited by t.dowe on 2009-10-20 01:45 PM
0 项奖励
回复