Sorce code and Doc for BUFFALO or other Monitor  for 68HC11

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Sorce code and Doc for BUFFALO or other Monitor  for 68HC11

10,143件の閲覧回数
IrajRafiei
Contributor I
Hello everybody
 
 Could everyone help me find sorce code and doc for BUFFALO or other Monitor  for 68HC11?
 
Special Thanks
I. Rafiei
ラベル(1)
0 件の賞賛
返信
4 返答(返信)

3,399件の閲覧回数
jkenney3
NXP Employee
NXP Employee

Iraj,

Here is the BUFFALO assembly file.

Jim Kenney

 

buf34.asm

Message Edited by t.dowe on 2009-10-20 01:46 PM
0 件の賞賛
返信

3,399件の閲覧回数
jkenney3
NXP Employee
NXP Employee

Iraj,

The S19 file. I changed the extension to .txt so that the system would take it.

Jim Kenney

 

BUF34.txt

Message Edited by t.dowe on 2009-10-20 01:47 PM
0 件の賞賛
返信

3,399件の閲覧回数
Alban
Senior Contributor II
Hi Jim,
 
From now S19 and S2 are authorized on all boards. Thanks for flagging this up.
 
Alban.
0 件の賞賛
返信

3,399件の閲覧回数
jkenney3
NXP Employee
NXP Employee

Iraj,

 

I was looking for something else when I stumbled across your e-mail.  I looked thru my archives and found the attached files.  The User Manual is for the HC11EVB, a low cost evalutation board offered in the mid to late 90's.  It came with BUFFALO (Bit User's Fast Friendly Aid to Logical Operation) in the EPROM.  The UM can be considered a BUFFALO user's manual as well.  I have also attached the assembly code and S19 file for ver 3.4. (Looks like the message board allows only one attachment at a time.  I will send the code seperately.)

These come with no warranty of any kind.  You may need to dust them off before you use them as they have been on my shelf since 2000.

Have fun!

Jim Kenney

 

11evbu.pdf

Message Edited by t.dowe on 2009-10-20 01:45 PM
0 件の賞賛
返信