Slow throughput for MC13213 SRB

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Slow throughput for MC13213 SRB

1,710 次查看
thngkl
Contributor I
I am using the MC13213 SRB for my project and i am using the packet mode for transmitting and receiving. The input to the transmitting side is a 11 bit data and new data arrives every 1ms. The SRB is supposed to send these data to the receiving side. However i realise that the throughput is too slow, meaning that the transmitter is not fast enough to process and send the data out every 1ms. What do i need to change in order to increase the processing speed?
标签 (1)
0 项奖励
回复
1 回复

774 次查看
NLFSJ
Contributor III
I am not very familiar with the device, but as the MC13213 reference manual say, the maximum throughput is 250 kbps. It means that the baudrate will depend on the amount of bytes that the application is transmitting, the data processing and the codification of the application. Unfortunately there is nothing to do in order to enhance the SMAC broadcast speed. Remember the MC13213 system is intended to monitoring and control application with a low baudrate needed.
 
Regards,
Nina
0 项奖励
回复